Example project couldn't be loaded into NUCLEO-L552ZE-Q
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-26 7:11 PM
STMicroelectronics ST-LINK GDB server. Version 5.6.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0-RC1
-------------------------------------------------------------------
ST-LINK SN : 066CFF353638425043092929
ST-LINK FW : V2J37M26
Board : NUCLEO-L552ZE-Q
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x472
Revision ID : Rev B
Device name : STM32L5xx
Flash size : 512 KBytes (default)
Device type : MCU
Device CPU : Cortex-M33
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_bkZXrr.srec
File : ST-LINK_GDB_server_bkZXrr.srec
Size : 7336 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 3]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.275
Verifying ...
Error: Data mismatch found at address 0x08000000 (byte = 0xFF instead of 0x00)
Error: Download verification failed
Encountered Error when opening /home/mq/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_1.4.0.202007081208/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-26 8:46 PM
Found the solution,since it promoted the STM32CubeProgrammer CLI malfunction, so I programed the .elf file in a isolated Prog tool:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-26 7:18 PM
I guess it was due to I set the "TZEN" enabled, but when I unchecked it in STM32Prog, it was prompted:
Error: Expected value for Option Byte "TZEN": 0x0, found: 0x1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-26 8:46 PM
Found the solution,since it promoted the STM32CubeProgrammer CLI malfunction, so I programed the .elf file in a isolated Prog tool: