2009-09-06 7:32 AM
Event driven low power mode
2011-05-17 4:22 AM
Hello.
In my application I would like to use stop mode, which will be exited by any edge (rising or falling) on GPIOA:3. However, I dont know what to do to exit from the stop mode. Here is all important lines (sequentially as CPU executes them) I use to initialize event-driven stop mode:Code:
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); EXTI_InitTypeDef EXTI_InitStructure; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Event; EXTI_InitStructure.EXTI_Line = EXTI_Line3; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising_Falling; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPD; GPIO_Init(GPIOA, &GPIO_InitStructure); PWR_EnterSTOPMode(PWR_Regulator_ON, PWR_STOPEntry_WFE); RCC_HSEConfig(RCC_HSE_ON); HSEStartUpStatus = RCC_WaitForHSEStartUp(); if(HSEStartUpStatus == SUCCESS) { RCC_PLLCmd(ENABLE); while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET); RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); while(RCC_GetSYSCLKSource() != 0x08); } Can you help me, please? I've read from Hitex document, that event driven low-power mode behaves similarily than interrupt driven, without setting interrupt and interrupt handler (so after wake-up, PC is loaded with the next instruction, not interrupt vector value).2011-05-17 4:22 AM
I need to mention, that if I modify preceding code to:
Code:
<BR>-- PWR_EnterSTOPMode(PWR_Regulator_ON, PWR_STOPEntry_WFE); <BR>++ __SEV(); <BR>++ PWR_EnterSTOPMode(PWR_Regulator_ON, PWR_STOPEntry_WFE); <BR>
then the result is still the same, e.g. even setting event by __SEV() before going to stop mode does not help, MCU goes to stop mode and never exits from. [ This message was edited by: juraj.vanco on 06-09-2009 20:28 ]