cancel
Showing results for 
Search instead for 
Did you mean: 

How should i create SVC calls from C?

marcus2399
Associate II
Posted on September 08, 2009 at 08:51

How should i create SVC calls from C?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
marcus2399
Associate II
Posted on May 17, 2011 at 13:22

In my hobby kernel, I have so far defined a few system calls. Currently I call them by doing inline assembly calls from a C program (I use gcc) or directly using the SVC instruction from an assembly program.

I am looking for a nice and compact way to call systems calls from C, i.e. a call like:

buffer = rtos_alloc(42);

should end up something like this after compilation:

mov r12, 1 # 1 = syscall id for alloc

mov r0, 42

svc

...

The return value from rtos_alloc is located in r0 which can then be assigned to ''buffer''.

I have tried a number of tricks using macros like:

#define rtos_syscall_1(CALL_ID, RET_TYPE, NAME, TYPE0, NAME0)

__attribute__ ((always_inline)) static inline RET_TYPE NAME(TYPE0 NAME0)

{

asm volatile(''mov r12, ''stringify(CALL_ID)''\n\t''

''mov r0, %0\n\t''

''svc\n\t'':: ''r'' (NAME0));

}

to define inline assembly functions, but I can't get it to work properly. Are there any better ways to do this?

picguy
Associate II
Posted on May 17, 2011 at 13:22

Go for clarity, not compactness.

Each function i.e. timer wait, wait for event, allocate etc should have its own subroutine.

Consider this (using IAR asm syntax) . . .

char* rtos_alloc(int arg)

{

// note: arg already in r0

asm (mov r12,#1); // allocate opcode

asm (svc 0);

// kernel returns address in r0

// ignore “no return value warning� (or turn it off)

}

This may take an extra stack level and a few extra lines of code. The compiler will push lr before calling rtos_alloc (unless it has already saved lr in the calling module.) You always have the bl rtos_alloc and the bx lr overhead. ‘Tiz a small price to pay for clarity.

It’s more work in your svc handler but you could use the svc code to say which function you are calling.

(But don’t inline a function that assumes r0 is set on entry. IAR noticed that arg was not used and optimized out loading r0.)

marcus2399
Associate II
Posted on May 17, 2011 at 13:22

Hi!

Thanks for your answer, I agree with you. Clarity is very important. Without considering the options, I was initially aiming for a compact inlined solution which, as you mention, might save a couple of instructions but increases complexity. GCC in this case pushes lr in the calling function anyway, so that wont give any extra cost.