cancel
Showing results for 
Search instead for 
Did you mean: 

Error word in RM0008: STM32F10x data for DAC channel2 to be loaded into DAC_DHR12LD [27:16] bits. What is correct DAC_DHR12LD[27:16] or DAC_DHR12RD[27:16]?

csocom
Associate II
Posted on July 13, 2018 at 10:29

STM32F10x DAC (stm32f_ref Manual_RM0008, page248)

........data for DAC channel2 to be loaded into DAC_DHR12LD [27:16] bits.

What is correct DAC_DHR12LD[27:16] or DAC_DHR12RD[27:16]?? error word

I think 

 Right about  DAC_DHR12R

D[27:16]

.
2 REPLIES 2
Posted on July 13, 2018 at 11:10

I agree, it should be talking about the Right Aligned positioning.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Imen.D
ST Employee
Posted on July 13, 2018 at 11:14

Hello 

CHUN.SOO_OK

 ,

Thanks for bringing this typo to our attention. 

This error will be fixed in the coming release of RM0008.

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen