2008-11-10 8:38 PM
Error in using FWLib 2.0.3 with Keil (Eval) version
2011-05-17 3:51 AM
Hi!
I just updated with the new version of FWLib 2.0.3 for Cortex M3. I just made a new project with the help of template given in the library for RTC Calender example. The project compiles fine. I turned the debug option from ULINK to Simulator and when I tried to simulate the code I got an error. Plz see attached images. I would be grateful if some one could help me :( Cheers, -Hassan2011-05-17 3:51 AM
Hi Hassan,
I believe that only the projects inside Keil Installation folder : ''C:\Keil\ARM\Boards\Keil\MCBSTM32 ''are supporting simulation features with µVision. Else you need a hardware board and a real silicon with Ulink to run the examples on real STM32 micro. Regards, STOne-32.2011-05-17 3:51 AM
I see! Yes probably this is the problem! Many thanks for the prompt reply.
Regards, -Hassan