cancel
Showing results for 
Search instead for 
Did you mean: 

Error in the F7 DISCO Documentation

cm600
Associate II
Posted on October 05, 2015 at 14:50

There is a very nasty error in the UM1907 - the net labels ARD_D5 and ARD_D10 are connected to PI.10 and PA.8 on the schematic on page 32

but on the schematic on page 29 AND in the table on page 19 the labels and the port pins are reversed.
1 REPLY 1
Posted on October 05, 2015 at 15:07

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/STM32F7%20Discovery%20Pins%20PA8%20and%20PI0%20are%20swapped%20on%20the%20Arduino%20header&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=138]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FSTM32F7%20Discovery%20Pins%20PA8%20and%20PI0%20are%20swapped%20on%20the%20Arduino%20header&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=138

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..