2015-11-11 8:02 AM
Hi everone, i have some problem with stm32f4 discovery. i use STLink-utility , when i try to connect to target, it always show ''Can not read memory. Disable read out protection and retry''. i was search in internet and it say that i should go to target->option byte -> read out protection level 0 , i was try and ST-Link Utility ''Could not set option byte, please reset the target and retry''.??? it mean pust reset button on stm32f4??? i did it but nothing, it still ''Can not read memory. Disable read out protection and retry''. Please help me
2015-11-11 8:31 AM
Can you access/erase the device if you jumper BOOT and VDD pins together?
2015-11-11 8:45 AM
Yes i did it, jumper BOOT0 to VDD and try to program, eraser, eraser sector, but it still say ''Read out protection is activated'' how can i disable it and program normal. But just one thing, when i program, it say that ''Read out protection is activated. Do you want to disable chip and program the chip'', i chose OK and it say ''Could not disable read out protection''
2015-11-11 9:35 AM
Did this board ever work correctly? What did you do prior to it failing, exactly?
Try a different cable. Try a different PC. Make sure you have current drivers and firmware. Describe your system in more detail.2015-11-12 4:07 AM
maybe i think it was died, before that i use 3.7v battery (battery for mobile) for 3v pin in stm32f4 ,i think stm32f4 have regular circuit on board so i do that.