2016-11-22 8:34 AM
Hello,
could someone explain me why CubeMX 4.17 generates two: void SystemClock_Config(void); (one static)/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void Error_Handler(void);
static void MX_GPIO_Init(void);
static void SystemClock_Config(void);
static void MX_DAC1_Init(void);
static void MX_DAC2_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_SPI1_Init(void);
And then calls it 2 times?
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
SystemClock_Config();
MX_DAC1_Init();
MX_DAC2_Init();
MX_USART2_UART_Init();
MX_USART3_UART_Init();
MX_SPI1_Init();
System info: Fedora 23 MCU:STM32F373RCTx
2016-11-23 12:46 AM
Hello,
Share your .ioc file to review your configuration and help you on this.Regards2016-11-23 3:31 AM
I added .ioc and main.c files
Best regardsBartek2017-05-05 12:19 AM
Hi
Balcerzak.Bartosz
,Sorry for the late response.
There is no more issue on the latest release. Please upgrade your CubeMX release with the latest.
BR. Eric