2013-07-16 5:24 AM
I have STM32F4-discovery board. And I use code from example to configure PWM output.
Chapter 14.4.9 TIMx capture/compare enable register (TIMx_CCER) of RM0090: Bit 0 CC1E: Capture/Compare 1 output enable. CC1 channel configured as output: 0: Off - OC1 is not active 1: On - OC1 signal is output on the corresponding output pin CCxE bit = 0 - Output Disabled (OCx=0, OCx_EN=0) I tried to use following configuration for TIM3 in PWM mode: TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Disable; TIM_OC1Init(TIM3, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable); But in fact output line is in high state. Is it possible to drive timer/pwm output line to low state? #discovery #stm32 #output #pwm2013-07-31 2:39 AM
The configuration should be similar to the following:
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;
TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low;
TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set;
TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset;
-Mayla-
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.