cancel
Showing results for 
Search instead for 
Did you mean: 

Downloading a binary file into STM32L

nanayakkaraan
Associate II
Posted on January 21, 2011 at 10:43

Downloading a binary file into STM32L

3 REPLIES 3
trevor23
Associate III
Posted on May 17, 2011 at 14:22

''STM32 utility is one such program but it doesnot work''

ST flash loader works for me. What is it that does not work for you?

Do you want to download over serial or USB or something else?

nanayakkaraan
Associate II
Posted on May 17, 2011 at 14:22

Hello Trevor,

Thanks for replying. :D

When I tried to program my STMicro using STM32 ST-LINK Utility, it says that ''Some flash sectors are protected'' and ''Readout Protection is Enabled''. When i tried to disable write and readout protection using option byte tab it could not be done.

Any suggestions to overcome this issue are highly appreciated.

Thank you.

trevor23
Associate III
Posted on May 17, 2011 at 14:22

So you are using ST Link (you didn't say in your OP). I don't use ST Link so I can't help. Can you confirm the way you want to connect to the device to download the binary firmware image (I presume it is firmware) e.g.

* Serial

* USB

* JTAG

* SWD

* Don't care

You could use ''ST flash loader'' with a serial or USB connection to the STM32