2014-11-19 10:04 PM
Hi,
We are thinking to develop a Memory Controller for External Memory . I have gone through the (RM0090 Reference manual) STM32F405xx/07xx, STM32F415xx/17xx, STM32F42xxx and STM32F43xxx advanced ARM ® -based 32-bit MCUs. In Synchronous transactions of Wave forms are not clear when compared with the Memory Datasheets. Which type of memory supports this type. I have attched the Doc same here. Page No:1552Thanks2014-11-20 06:11 AM
Why would you attach a data sheet that's public available rather that just cite the download? If you have issues with diagrams, then mark them up and attach the image.
Synchronous SRAM?