2012-02-18 09:08 AM
I am able to open, compile and download both supplied projects from ST for the STM32L-DISCOVERY Framework. When running in DEBUG mode when the debugger excecutes the function Icc_run() at about line 221 in the AN3413 Current consumption.......... I get a STLinkIII error message ''Internal command error'' then ''Error attempting to read 64bytes from 0x00000000''
Any help will be appreciated.