cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32F446 not have full-duplex I2S?

Bumsik Kim
Senior
Posted on December 02, 2016 at 04:43

Hello, I am designing a project using STM32F446, hoping to get more performance than STM32F401/411.

After some research and trial and error, it looks like this MCU does not support full duplex I2S. I could not find I2S_SDext in the datasheet.

Is that correct this one does not support full-duplex I2S communication? Then how can I set I2C_SD pin as input or output?
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User
Posted on December 02, 2016 at 10:23

You are supposed to use SAI for I2S in the newer 'F4/'F7.

JW

slimen
Senior
Posted on December 02, 2016 at 10:33

Hello,

You should refer to your reference manual for more clarification.

Regards

Radek RIPA
ST Employee
Posted on December 05, 2016 at 19:00

Hello 

The I2S on STM32F446 which is shared with SPI is only half duplex(written in reference manual). 

The full duplex I2S is managed over newer SAI periphery.

Best regards

Radek

Bumsik Kim
Senior
Posted on December 19, 2016 at 01:09

Oh I didn't know the new SAI interface.

Thanks for you help.