2018-05-08 10:54 AM
HI.I recently bought myself a board with a STM32f411 nucleo. And there was a problem in the fact that CUBEMX hovered and did not close it. What should I do? Thank you in advance!
2018-05-09 2:21 AM
Hi
valik250403
,there was a problem in the fact that CUBEMX hovered and did not close it
CUBEMX version are you using?
Maybe you shouldclean your cache and try again
Could you please give more details about your issue?
-Nesrine-
2018-05-09 2:37 AM
I'm using version 4.24.0. And the thing is when I open the project and start generating the code for STM32F411RE, my CUBEMX hangs. When I select another STM32 everything works normal without freezes.
2018-05-09 4:44 AM
Hi
valik250403
,Could you please try to use the last CUBEMX version (4.25) and tell us if the issue still again.
-Nesrine-
2018-05-09 7:35 AM
Same.
2018-05-09 7:38 AM
Hi
valik250403
,This is reported to our MX team for check!
-Nesrine-
2018-05-09 7:40 AM
Good. I'm waiting.
2018-05-10 3:32 AM
Hi
valik250403
Could you please attach the ioc, it will help for debug
2018-05-10 6:49 AM
Here is the file
________________ Attachments : stmproject.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxXp&d=%2Fa%2F0X0000000b0Q%2FlM3V6c_2fZVY4kN6t18M.qOFZB5VrDQ2qaJnNe0JBCc&asPdf=false2018-05-11 4:24 AM
Using your ioc the project is well generated and compiled correctly, it seems that there is an issue related to your install or PC.
Could you please put the log file of CubeMX in a comment, you will find it under /user_folder/.stm32cubemx/STM32CubeMX.log