Skip to main content
Associate II
October 10, 2024
Solved

DMA mapping for STM32F407 series

  • October 10, 2024
  • 2 replies
  • 5873 views

What is the meaning of These requests are available on STM32F42xxx and STM32F43xxx only for DMA1 and These requests are available on STM32F42xxx and STM32F43xxx for DMA2.
What should ı use for the mapping ?

tinkerer_of_universe_0-1728549436946.png

 

Best answer by mƎALLEm

@tinkerer_of_universe wrote:

Which channel should I choose for transferring CDR register data?


CDR on which ADC? as I said, each one has its channel and stream as shown in the table.

 


@tinkerer_of_universe wrote:

Does this sentence have no relevance to STM32F407
These requests are available on STM32F42xxx and STM32F43xxx only for DMA1 and These requests are available on STM32F42xxx and STM32F43xxx for DMA2.


This note is related to some peripheral mappings:

SofLit_0-1728551169495.png

So these requests are available only on STM32F42xxx and STM32F43xxx products.

2 replies

Andrew Neil
Super User
October 10, 2024

For some reason, the forum can't display your image:

AndrewNeil_0-1728549235630.png

Note that you can just paste straight into the post so that the image is immediately visible.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
October 10, 2024

Thank you ı fix the image

 

mƎALLEm
ST Technical Moderator
October 10, 2024

Hell @tinkerer_of_universe and welcome to the community,

For example, if you want to trigger DMA transfer using ADC3 end of conversion, you need to select Stream 0 / Channel 2.

SofLit_1-1728550074683.png

Example from HAL:

 

hdma_adc.Instance = DMA2_Stream0;
hdma_adc.Init.Channel = DMA_CHANNEL_2;

 

For more details, please review the AN4031  "Using the STM32F2, STM32F4 and STM32F7 Series".
DMA controller 

Figure 1. DMA block diagram

SofLit_0-1728550326200.png

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate II
October 10, 2024

Which channel should I choose for transferring CDR register data?
also
Does this sentence have no relevance to STM32F407
These requests are available on STM32F42xxx and STM32F43xxx only for DMA1 and These requests are available on STM32F42xxx and STM32F43xxx for DMA2.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
October 10, 2024

@tinkerer_of_universe wrote:

Which channel should I choose for transferring CDR register data?


CDR on which ADC? as I said, each one has its channel and stream as shown in the table.

 


@tinkerer_of_universe wrote:

Does this sentence have no relevance to STM32F407
These requests are available on STM32F42xxx and STM32F43xxx only for DMA1 and These requests are available on STM32F42xxx and STM32F43xxx for DMA2.


This note is related to some peripheral mappings:

SofLit_0-1728551169495.png

So these requests are available only on STM32F42xxx and STM32F43xxx products.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.