2016-04-26 4:13 AM
Hi
I have a problem with the DMA Interrupt on a nucleo stm32f4 Everytime the Nucleo goes into an Infinite_Loop
1.
.section .text.Default_Handler,
''ax''
,%progbits
2.
Default_Handler:
3.
Infinite_Loop:
4.
b Infinite_Loop
5.
.size Default_Handler, .-Default_Handler
my main.cpp is this one:
#include ''mbed.h''
#include ''globals.h''
UART_HandleTypeDef huart2;
DMA_HandleTypeDef hdma_usart2_tx;
void DMA1_Stream6_IRQHandler(void);
void
SystemClock_Config(
void
);
static
void
MX_GPIO_Init(
void
);
static
void
MX_DMA_Init(
void
);
void
test(DMA_HandleTypeDef* dma){
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5,GPIO_PIN_RESET);
char
buffer[] =
''12345678901234567890123456789000000''
;
HAL_DMA_Start_IT(&hdma_usart2_tx, (uint32_t) &buffer, (uint32_t)&(USART2->DR),
sizeof
(buffer));
USART2->CR3 |= USART_CR3_DMAT;
}
void
HAL_UART_MspInit(UART_HandleTypeDef* huart)
{
GPIO_InitTypeDef GPIO_InitStruct;
if
(huart->Instance==USART2)
{
/* USER CODE BEGIN USART2_MspInit 0 */
/* USER CODE END USART2_MspInit 0 */
/* Peripheral clock enable */
__USART2_CLK_ENABLE();
/**USART2 GPIO Configuration
PA2 ------> USART2_TX
PA3 ------> USART2_RX
*/
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* Peripheral DMA init*/
hdma_usart2_tx.Instance = DMA1_Stream6;
hdma_usart2_tx.Init.Channel = DMA_CHANNEL_4;
hdma_usart2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_usart2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_usart2_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_usart2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_usart2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_usart2_tx.Init.Mode = DMA_NORMAL;
hdma_usart2_tx.Init.Priority = DMA_PRIORITY_LOW;
hdma_usart2_tx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_usart2_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_usart2_tx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_usart2_tx.Init.PeriphBurst = DMA_PBURST_SINGLE;
hdma_usart2_tx.XferCpltCallback = test;
HAL_DMA_Init(&hdma_usart2_tx);
__HAL_LINKDMA(huart,hdmatx,hdma_usart2_tx);
/* USER CODE BEGIN USART2_MspInit 1 */
/* USER CODE END USART2_MspInit 1 */
}
}
void
MX_USART2_UART_Init(
void
)
{
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
HAL_UART_Init(&huart2);
}
int
main() {
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Initialize all configured peripherals */
MX_GPIO_Init();
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5, GPIO_PIN_SET);
MX_DMA_Init();
MX_USART2_UART_Init();
char
buffer[] =
''12345678901234567890123456789000000''
;
HAL_DMA_Start_IT(&hdma_usart2_tx, (uint32_t) &buffer, (uint32_t) &(USART2->DR),
sizeof
(buffer));
USART2->CR3 |= USART_CR3_DMAT;
while
(1){}
}
void DMA1_Stream6_IRQHandler(void)
{
/* USER CODE BEGIN DMA1_Stream6_IRQn 0 */
HAL_NVIC_ClearPendingIRQ(DMA1_Stream6_IRQn);
/* USER CODE END DMA1_Stream6_IRQn 0 */
HAL_DMA_IRQHandler(&hdma_usart2_tx);
/* USER CODE BEGIN DMA1_Stream6_IRQn 1 */
/* USER CODE END DMA1_Stream6_IRQn 1 */
}
#stm32 #dma #interrupt #handler
2016-04-26 4:29 AM
void DMA1_Stream6_IRQHandler(void)
cheers,Torsten