cancel
Showing results for 
Search instead for 
Did you mean: 

DMA FIFO level

cahmep
Associate
Posted on March 09, 2015 at 08:39

Please, confirm

my assumption: it is typing error in RM0090? Register DMA_SxFCR STM32F4xx

  • Bits 1:0 FTH[1:0]: FIFO threshold selection

  • These bits are set and cleared by software.

  • 00: 1/4 full FIFO

  • 01: 1/2 full FIFO

  • 10: 3/4 full FIFO

  • 11: full FIFO

  • These bits are not used in the direct mode when the DMIS value is zero.

  • These bits are protected and can be written only if EN is ‘1’

Must be EN = 0?P.S.

On this forum

, it is impossible to format the message

.

This is the worst

that

can be found

.

Developer

Wake up!

3 REPLIES 3
Posted on March 09, 2015 at 08:58

>

Must be EN = 0?

Yes. Nice catch.

> P.S.

On this forum

, it is impossible to format the message

.

This is the worst

that

can be found

.

Developer

Wake up!

This is a Micro$oft product and it's very unlikely ST can do anything about it. Welcome to the club. Some of the frustration can be relieved by adding a ''worst forum software ever'' tag below... :)

JW

AvaTar
Lead
Posted on March 09, 2015 at 12:59

This is a Micro$oft product and it's very unlikely ST can do anything about it

.

 

Not sure about that. Once ST had the choice, to either have a proper forum software, or something from Micro$oft. They still could migrate ...

And while I don't like the above mentioned abuse NSA-bedfellow, there is more blame to put on ST. To use 'SharePoint' as user-forum software, is, euphemistically said, a little bit 'creative'.

childresss
Associate II
Posted on March 10, 2015 at 23:00

1970's ''No one ever got fired for choosing IBM''.

1990's- ''No one ever got fired for choosing Microsoft''.

My big ole company drinks the MS kool-aid. Unfortunately, that includes the god-awful software called Sharepoint.