Skip to main content
Associate III
September 3, 2024
Question

DMA channel1 Stream 0-7 which channel to choose

  • September 3, 2024
  • 6 replies
  • 3129 views

Hi i m working on H732 timer1 as PWM and its working fine, but when I try to implement DMA on timer1, there is no waveform. I enclosed the DMA code below, as I declare an array of 10 PWM duty cycle values..

i suspect it's the Timer1 channel1 stream that's causing the issue, can anyone advise which stream to choose? (stream 0-7 ? )

  HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, (uint32_t *)pwmAll, 10);  

 

StanJerm_0-1725327735894.png

 

This topic has been closed for replies.

6 replies

TDK
September 3, 2024

The streams within a DMA are equivalent in all important aspects. In any case, choosing a different stream will not fix the problem.

The problem is likely that the array is not in a location that the DMA can access.

DMA is not working on STM32H7 devices - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."
StanJermAuthor
Associate III
September 3, 2024

***! Why did the H7 series got this DMA issue? It looks like I have to migrate to F7 series? 

TDK
September 3, 2024

> ***! Why did the H7 series got this DMA issue? It looks like I have to migrate to F7 series? 

Did you read the linked article? It doesn't sound like you did.

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
September 3, 2024

Because it's very complicated. 

And that's because that's the only way to achieve the high operational speed. 

JW