2013-02-21 6:21 AM
Hi
I am using the stm3240G eval board. The DMA works fine for an image resolution of 300xBut when I increase the resolution I do not get any image. I am using DMA in circular buffermode and have tweaked the codes I have got from this forum. There are two function I have doubtson.
void Capture(void)
{
/* Disable any old interrupts before enabling DMA
WARNING: This is not specified in the reference manual,
but MUST be done before enabling stream. */
DMA_ClearITPendingBit ( DMA2_Stream1, DMA_IT_TCIF1 |
DMA_IT_HTIF1 |
DMA_IT_TEIF1 |
DMA_IT_DMEIF1 |
DMA_IT_FEIF1 );
DMA2_Stream1->M0AR = Bank1_SRAM2_ADDR;
DMA_DoubleBufferModeConfig(DMA2_Stream1, Bank1_SRAM2_ADDR + ( 0xffff * 4 ), DMA_Memory_0);
/* Enable DMA transfer */
DMA_Cmd(DMA2_Stream1, ENABLE);
/* Wait for DMA to start up */
while ( DISABLE == DMA_GetCmdStatus ( DMA2_Stream1 ) );
/* Enable DCMI interface */
DCMI_Cmd ( ENABLE );
DCMI_ITConfig ( DCMI_IT_FRAME, ENABLE );
/* Start Image capture */
DCMI_CaptureCmd ( ENABLE );
while ( 0 == DCMI_GetFlagStatus ( DCMI_FLAG_FRAMERI ) );
DCMI_CaptureCmd ( DISABLE );
DCMI_Cmd ( DISABLE );
DMA2_Stream1->M0AR = Bank1_SRAM2_ADDR;
DMA_DoubleBufferModeConfig(DMA2_Stream1, Bank1_SRAM2_ADDR + ( 0xffff * 4 ), DMA_Memory_0);
DMA_Cmd ( DMA2_Stream1, DISABLE );
/* Wait for DMA to stop */
while ( ENABLE == DMA_GetCmdStatus ( DMA2_Stream1 ) );
LCD_DisplayStringLine(LINE(4), ''Capture function completed '');
return;
}
The next is the IRQ for DMA.
void DMA2_Stream1_IRQHandler(void)
{
static uint8_t ucCount = 0;
LCD_DisplayStringLine(LINE(11), ''DMA Interrupt'');
DMA_ClearITPendingBit ( DMA2_Stream1, DMA_IT_TCIF1 );
ucCount++;
// The first interrupt moves the initial buffer out by 0x7fff8
if ( 1 == ucCount )
{
DMA2_Stream1->M0AR = Bank1_SRAM2_ADDR + ( 0xFFFF * 8 );
}
// The third interrupt
else if ( 3 == ucCount )
{
DMA2_Stream1->M0AR = Bank1_SRAM2_ADDR;
DMA2_Stream1->M1AR = Bank1_SRAM2_ADDR + ( 0xFFFF * 4 );
ucCount = 0;
}
}
The above functions work alright for a image resolution of 300x200 but fails for higher
resolutions. One important thing is that the DMA interrupt is never called. I can understand
this for 200x300 image but for higher resolution I was expexting the interrupt to occur. But
it never happened. By higher resolution I mean 1000x1000.
I would be really obliged if someone could take a look and point out to me where I am going
wrong.
Thanks in advance.