cancel
Showing results for 
Search instead for 
Did you mean: 

DMA的�?�?�模�?和FIFO有什么关系啊,是一个�?�?嘛

L罗.1
Associate II
 
1 REPLY 1
KDJEM.1
ST Employee

Hello @LSL 罗​,

Thanks to develop your posts in English so it helps us, and the users of our community understand your question and try to help you.

I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.  

Here is the translation of your post using Google translate:

What is the relationship between DMA burst mode and FIFO? It means the same thing.

In STM32F7 MCU, burst mode is only available when FIFO mode is enabled.

When setting burst mode, the FIFO threshold should be compatible with burst size.

For more explanation, I advise you to take a look at the application note: AN4031 Using the STM32F2, STM32F4 and STM32F7 Series DMA controller.

Also, you can attend the available training in the ST website.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thank you

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.