cancel
Showing results for 
Search instead for 
Did you mean: 

distinguish different stm32f407

shark
Senior
Posted on November 10, 2014 at 03:39

I have developed same binary code that can run on both 100 pins and 176 pins version of stm32f407. How can I distinguish these mcu by checking registers or memory locations? Their cpuid are same?

thanks.

#cpuid
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on November 10, 2014 at 04:31

You can't. They share the same die bonded out differently.

You can read the tested Flash Size.

You can strap pins externally, either to id the chip, or the pcb to which it is attached.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..