2013-05-25 3:35 PM
Hi,
is it possible to sample GPIOA Bit7-0 into SRAM as byte and to have kind of ''Clk'' nonPWM output on other GPIO , with higher speed than 20MHz on STM32F103 72MHz ? this gives me 10MHz clk output on PC2: Buffer_ptr=(uint8_t *)Buffer; while( 1 ) { *(Buffer_ptr++)=(uint8_t)GPIOA->IDR; GPIOC->ODR = GPIO_Pin_2; if(Buffer_ptr>=(uint8_t *)(Buffer+20000)) break; GPIOC->ODR = 0; } Thank You for all replies2013-05-25 5:00 PM
DMA transfer of a GPIOx->ODR, triggered by a TIM, output of same trigger pulse. Speed of the APB may be a limiting factor here. Consider a different part from the F2/F4 series.
2013-05-26 12:05 AM
i tried this with DMA:
Buff_PC2[0]=0; Buff_PC2[1]=GPIO_Pin_2; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(&GPIOC->ODR); DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)Buff_PC2; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure.DMA_BufferSize = 2; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA2_Channel1 , &DMA_InitStructure); TIM_TimeBaseStructure.TIM_Period = 1; TIM_TimeBaseStructure.TIM_Prescaler = 0x00; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit( TIM8, &TIM_TimeBaseStructure); TIM_UpdateRequestConfig( TIM8, TIM_UpdateSource_Regular ); DMA_Cmd( DMA2_Channel1, ENABLE); TIM_Cmd( TIM8, ENABLE); this generates 600kHz, did i make mistake somewhere in initialization ?