cancel
Showing results for 
Search instead for 
Did you mean: 

Different behaviour on using memcpy on external SDRAM with different addresses

jimmii
Senior II

Hi

I'm using a STM32H753 with external SDRAM connected to FMC.

I'm working with Keil and the compiler is armclang.

This is my MPU configuration for the SDRAM (base address is 0xC0000000) :

MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = 0xC0000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_64MB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;

This code initializes the MPU so that the SDRAM memory area is considered as Normal Memory type instead of Device Memory type. This disables the access alignment restrictions.

When I use memcpy with following code, everything is copied correctly:

volatile uint32_t len = 10;
uint8_t* src = (uint8_t*)0xc0000002;         // 2-byte aligned
uint8_t* dst = (uint8_t*)(0xc0000002 + 20);  // 2-byte aligned
memcpy(dst, src, len); // ok

0693W000007DsVWQA0.png 

But with following addresses (src 2byte aligned and dst 4byte aligned):

src = (uint8_t*)0xC0000002;         // 2-byte aligned
dst = (uint8_t*)(0xC0000002 + 22);  // 4-byte aligned
memcpy(dst, src, len);

This is the result of the memory after memcpy:

0693W000007DsV7QAK.png 

Memcpy does not have any problems when using internal RAM.

Is this a bug in memcpy? Is my MPU configuration wrong?

Please advise.

Thanks a lot.

/jimmii

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User

And what happens if you memcpy first from SDRAM offset 0x02 to internal RAM, and the from internal RAM to SDRAM offset 0x18?

JW

Hi @Community member​ 

Thanks. When I'm copying from external to internal RAM and then back to external everything is ok. Data is correct.

Do you have any assumptions?

/jimmii

waclawek.jan
Super User

No ideas.

You may want to contact ST directly, through FAE or the web support form.

JW

Thanks anyway.