2015-09-01 07:46 AM
Hello,
I have a program running on a STM3220G-EVAL board with the USB-HS by the ISP1705 PHY and its running ok. Now, I have to change to the USB3300 and I'm trying with the board Open407V-D and the USB3300 ULPI and it's not running. The problem, I think, is some difference between the ISP1705 and the USB3300 but I can't find it!!! Someone can help me?? I was looking for in internet but I couldn`t find anything. Thanks #usb3300-isp1705-stm3220g-eval2015-09-01 11:22 PM
I found the problem.
It was the ST's Pinout.