Skip to main content
FSHAI.1
Associate
April 10, 2023
Question

Did you ever experiance a situation in which once the controller is powered, it look like there is some short inside the chip and I get a samll hole in the case and the controlle is dead and it is a short to the board ?

  • April 10, 2023
  • 5 replies
  • 1357 views

..

This topic has been closed for replies.

5 replies

S.Ma
Principal
April 10, 2023

Not so far. If you apply wrong voltages/ground to the package pinout, you may be able to destroy any electronic chip. To check if a pin is still connected to the chip, you may use a multimeter in diod check mode between a pin and ground for example.

Tesla DeLorean
Guru
April 10, 2023

If you create a conduction path through the chip, the bond wires can typically carry quite a lot of current, certainly enough to burn holes and melt plastic.

If this is happening a lot, I'd look carefully at the design.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
FSHAI.1
FSHAI.1Author
Associate
April 11, 2023

Hi Tesla,

Thnaks, the thing is that I've assembled already 10 boards in which everything was fine, then somthing happend while bring up with one of the boards and I've notices the controller is not working so I've replaced it with a new one and when powering it up it blowed. If for some reason one of the controller inputs is connected directly to 5V (one of the buffres become a "short") Can it cause the ST to "burn" ?

Thnaks Shai

Bob S
Super User
April 11, 2023

Which CPU are you using?

Depends on which pin and which STM32 part. Most pins are 5V tolerant, though NOT with 5V applied before the CPU has 3.3V power (typically the max voltage spec is VCC+4V, or something like that).

But is the pin is shorted to 5V and then configured as an output - that might damage the chip. But that assumes you were able to load firmware. On an un-programmed part, the internal bootloader will run, but that doesn't typically enable output pins and drive them low. It DOES enable output pins and drive them high (UART pins, for example). So if those pins were shorted to GND it might damage the part. See AN2606 for the pins used by the bootloader for your CPU.

Pull the 2nd blown CPU then check all the connections to the CPU for suspicious voltages or hard shorts to GND.

Bob S
Super User
April 11, 2023

Could the CPUs (or some other component) have been installed in the wrong orientation? No tlikely if buid on pick-n-place equipment, unless someone hand-loaded the parts into the tape.