cancel
Showing results for 
Search instead for 
Did you mean: 

Detect internal wake from RTC

x4ce
Associate III

Hello,

I am using RTC internal wake [10 sec] using the following code:

void go_to_sleep(void) { HAL_SuspendTick(); HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 10, RTC_WAKEUPCLOCK_CK_SPRE_16BITS); HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI); HAL_RTCEx_DeactivateWakeUpTimer(&hrtc); SystemClock_Config(); HAL_ResumeTick(); }

 

After that use following code to detect the source of the wake:

__HAL_RCC_PWR_CLK_ENABLE(); /* Check and Clear the Wakeup flag */ if(__HAL_PWR_GET_FLAG(PWR_FLAG_WUFI) != RESET) { __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUFI); printf("RTC Wake Up flag set\n\r"); } /* Clear source Reset Flag */ __HAL_RCC_CLEAR_RESET_FLAGS();

 

The device wakes up every 10 seconds and toggles the LED but WUFI is not detected/ set. The RTC is set to WakeUp through Internal WakeUp so I believe WUFI should be set.

Please suggest what could be wrong.

 

Thanks

 

 

0 REPLIES 0