cancel
Showing results for 
Search instead for 
Did you mean: 

Demo app already installed on STM32L476-DISCO

Thomas Pasch
Associate
Posted on June 03, 2017 at 08:20

Hello,

I fiddled around with an stm32l476 discovery board. Is there a way to reinstall the demo app originally installed on the device? Is there a place where I could find the source code?

Kind regards,

aanno

Btw, the board is embed.org ready. But there seems to be no build in IP connection (WiFi, Lan). What is the proposed way to get the board Iot cloud connected?

#demo-application #stm32l476
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
LMI2
Lead
Posted on June 03, 2017 at 16:48

Yes. The demo program is in the file stm32cube_fw_f7_v170.zip. It comes with the STM32CubeMX.