2013-10-12 9:10 AM
I want to write function using timer 2 for have millisecond in STM32F103 I just don't know why this doesn't work!
TIMER2 config: void config_TIM2() { NVIC_InitTypeDef NVIC_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStructure; /* Enable the TIM2 gloabal Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = TIM_CKD_DIV1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; /* Initialize TIM2 Interrupt */ NVIC_Init(&NVIC_InitStructure); /* TIM2 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); /* Time base configuration */ TIM_TimeBaseInitStructure.TIM_Period = 360 - 1; TIM_TimeBaseInitStructure.TIM_Prescaler = 10 - 1; TIM_TimeBaseInitStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseInitStructure.TIM_CounterMode = TIM_CounterMode_Up; /* Initialize TIM2 */ TIM_TimeBaseInit(TIM2, &TIM_TimeBaseInitStructure); /* TIM IT enable */ TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); /* TIM2 enable counter */ TIM_Cmd(TIM2, DISABLE); } here I count down each milliseconds : void TIM2_IRQHandler() { TIM_ClearITPendingBit(TIM2, TIM_FLAG_Update); ntime--; } Here wait until nms milliseconds void delay_ms(u16 nms) { ntime = nms; TIM_Cmd(TIM2, ENABLE); while (ntime); TIM_Cmd(TIM2, DISABLE); } #timer #stm32 #interrupts2013-10-12 10:02 AM
Doesn't work how? Doesn't generate interrupts, wrong rate?
Right now the frequency is probably wrong if APB1 is at 36 MHz, as the TIMCLK will be 72 MHz I don't see where ntime is defined, hopefully it's ''volatile'' I might use SysTick with a 1 ms tick, and count time from there, or a free running timer