2012-09-26 04:15 AM
Hi! All,
I am willing to debug stm32l152rbt6 in stm32l-discovery board via ST-LINK/V2(A201206) Debugger. Can any one post me the procedure. Even though the stm32l-discovery board contains in built SWD, but i don't want to use this, because i am planning to prepare microcontroller boards without SWD, in that context ST-LINK/V2(A201206) Debugger is more helpful. #debug-stm32-using-st-link/v2 #rtfm2012-09-26 04:24 AM
From the manuals and schematics it's should be pretty evident how to attach an external debugger. Hint: look at the CN3 jumpers.