2013-10-14 3:38 AM
Hello together,
I got an STEVAL-CCM001V2 evaluation board. This Board has an TFT-Display and some touch-keys to control the function of the board. The board has an micro-SD card slot and you could watch pictures on the sd-card over the usb-connection.When I got the board Iconnected it with my pc and after the driver was installed I could see the data on the card and watch pictures from the card on the board. Also I could configure the time and date in the menue, I would say basically the normal function.So in the package there is also the software of the application, and I have the ST-Link/V2 and I wanted to debug the application over SWD and my ST-LINK/V2.So I compiled direct the project from the CD and flashed it down into the controller and when I started it, the display was white an the usb-port is registered in the pc and after a few seconds the usb-port disappears in the pc.I think the software which is delivered with the package doesen't met to board or there is a new version which is different.If I could get the working programming file I could put the board in the delivered state but now it does not work anymore.Is there anybody who knows the board or has similar experiences?Thanks2013-10-14 4:53 AM
Should perhaps have used the ST-Link utilities to have saved the original firmware first? Maybe you can find some other user with the board? Not seeing much traffic in that regard.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.