Debug STM32H747 dual core application with Keil uVision
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-23 4:42 AM
I am trying to debug a dual core processor (STM32H747) with Keil uVision and ST-LInk V3. The application is running successfully on both cores but when i try to debug the CM4 core while the CM7 core is already running in another debug session, the CM4 core stops when i start the debug session. I am able to start the CM4 within the debug session.
I wonder why this is not working because if i use an old ULINK2 debugger i am able to connect to the CM4 core without stopping (Debug setting: Connect without Stop used).
For the ST-LINK the following debug options are still disabled at the Keil uVision.
- Load Application at Startup
- Connect Normal
- Update Target before Debugging
Best regards
Labels:
- Labels:
-
DEBUG
-
STM32H7 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0