2022-11-08 7:47 AM
Hi,
Since a few minutes, I'm experiencing a problem in CubeIDE v1.10.1 when I try to debug my code. Here is the message I'm getting in the console window:
File download complete
Time elapsed during download operation: 00:00:00.818
Verifying ...
Download verified successfully
Failed to assign value 8000f4d, to register 0
Failed to assign value 2000fff8, to register 0
Failed to assign value 8001070, to register 0
The same code on Mac is running and debugging properly.
Any clue to solve the problem?
Thanks a lot!
2022-11-08 10:05 AM
Seems to be a comms failure.
Check quality of USB cables, avoid hubs and docking stations.
Make sure part is not going into low-power states.
STM32L432KC on a custom board, or some ST board?
2022-11-09 1:07 AM
It is a ST Nucleo board.I followed your advice but it didn't improve the situation. Therefore I desinstalled CubeIBE and will give a try with a fresh install.
Thanks!
2023-01-25 7:20 AM
Hello,
I have the same problem. I tried two programmers, two USB cables, and two boards (different MCU) reinstalling everything (cubeMX, cubePROG, cubeIDE) and the problem still persists.
I have no idea what to try now, maybe another PC? But it's not a solution.
Thank you,
George
2023-03-10 3:28 PM
I have the same issue during debugging, I keep having to go back to compare current "...launch" file to working ".launch" files for my program and it sometimes fixes the issue.