cancel
Showing results for 
Search instead for 
Did you mean: 

Dear support I have a problem reading the data from the hyperram octal memory, can anyone help me please?

AAree.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
ChahinezC
Lead

Hello @AAree.1​,

What is the MCU/board you are using ? And what kind of problem you are facing?

Regards,

Chahinez.

ChahinezC
Lead

Hi,

Unfortunately, your question lacks clarity and details. If you want to get quick technical support, it is important to provide more details concerning your problem, the setup you are working with, the steps you have undertaken to solve it, etc. I recommend you this short tutorial: How to Post.

Kindly,

Chahinez.

AAree.1
Associate II

Hi

Thank you for answering me, I use the STM32H735

Alexi.

This is a technical venue, expect to provide enough detail about your problem that someone unfamiliar with your work would need to understand it.

What memory chip is the H735 connected too?

What board is this on? A board you designed, or an ST model?

If custom, perhaps add a schematic.

Related code you're using to initialize.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ChahinezC
Lead

Hello @AAree.1​,

Are you working on ST board or your own design using the STM32H735 chip?

What kind of problem you are facing with the data read?

Thank you.

Chahinez.

AAree.1
Associate II

Thank you for answering me.

I am using the STM32H735 discovery, the problem is that the data I am reading is not the same written, it's like the data is totally corrupted. I have generated the code with STM32CUBEMX.

here is the configuration of the hyperbus memory:

0693W00000bhRUCQA2.jpg

LCE
Principal II

I'm using the same board, works like a charm, memory-mapped mode.

Make sure that it's not running at more than 100 MHz.

Here's my almost non-HAL setup:

OSPI_HandleTypeDef hOspi1;
OSPI_HandleTypeDef hOspi2;
 
/* OCTOSPI2 basic init function */
/* input clock is 1/2 HCLK */
uint8_t OctoSpi2_Init(void)
{
	uint8_t u8RetVal = 0;
 
	/* Initialize OctoSPI ----------------------------------------------------- */
	hOspi2.Instance = OCTOSPI2;
 
	/* clock & GPIO initialization */
	HAL_OSPI_MspInit(&hOspi2);
 
	/* start OFF */
	OCTOSPI2->CR = 0;
 
/* device config registers
 *	DCR1 .. DCR4
 */
 
	/* DCR1:
	 *	MTYP 	= 100	Hyperbus memory mode
	 *	DEVSIZE
	 *	CHST
	 *	DLYBYP 	= 0		delay block is used
	 *	FRCK 	= 0		no free running clock
	 *	CKMODE 	= 0		clock low when idle
	 */
	OCTOSPI2->DCR1 =	OCTOSPI_DCR1_MTYP_2 |
						((OSPI_HYPERRAM_SIZE - 1) << OCTOSPI_DCR1_DEVSIZE_Pos) |
						((OSPI_HYPERRAM_NCS_HITIME - 1) << OCTOSPI_DCR1_CSHT_Pos);
 
	/* DCR2:
	 *	WRAPSIZE 	= 0 	wrapped read OFF
	 *	PRESCALER 	= 1 	divide by 2 -> 100 MHz = max at 3.3V
	 */
	OCTOSPI2->DCR2 = 	(OSPI_HYPERRAM_WRAP_ZERO << OCTOSPI_DCR2_WRAPSIZE_Pos) |
						((OSPI_HYPERRAM_CLK_DIV - 1) << OCTOSPI_DCR2_PRESCALER_Pos);
 
	/* DCR3:
	 *	CSBOUND 	= 23 	set to 2^n memory size
	 *	MAXTRAN 	= 0 	unused
	 */
	OCTOSPI2->DCR3 = 	(OSPI_HYPERRAM_CSBOUND << OCTOSPI_DCR3_CSBOUND_Pos);
 
	/* DCR4:
	 *	REFRESH 	= 500 	NCS must be released, even for PSRAM for internal refresh
	 */
		OCTOSPI2->DCR4 = 	OSPI_HYPERRAM_REFRESH;
 
 
/* CR: control register
 *	no polling
 *	no interrupts
 *	FMODE 	= 0		indirect mode, set to memory-mapped mode later
 *	FTTHRES	= 4		FIFO threshold
 *	FSEL 	= 0		nc in octal mode
 *	TCEN 	= 0		no timeout counter
 *	DMAEN 	= 0		no DMA
 *	ABORT 	= 0		no ABORT request
 *	EN 		= 0		ENable set later
 */
	OCTOSPI2->CR =	((OSPI_HYPERRAM_FTHRES - 1) << OCTOSPI_CR_FTHRES_Pos);
 
/* TCR: timing config
 *	SSHIFT 	= 0 	no read sample shifting
 *	DHQC 	= 1 	delay hold quarter cycle ON
 *	DCYC 	= 0 	dummy cycles between readd addr & data
 */
	OCTOSPI2->TCR = 	OCTOSPI_TCR_DHQC |
						(OSPI_HYPERRAM_DCYC << OCTOSPI_TCR_DCYC_Pos);
 
/* Hyperbus configuration
 *	memory-mapped mode configuration
 *	CR, DCR1, CCR, WCCR, DLR, AR
 */
 
	/* HLCR: HyperBus latency configuration register
	 *	TRWR[7:0]	= x		read write recovery time
	 *	TACC[7:0]	= y		yccess time
	 *	WZL			= 0		latency on write access
	 *	LM			= 1		fixed latency
	 */
	OCTOSPI2->HLCR = 	(OSPI_HYPERRAM_RW_REC_TIME << OCTOSPI_HLCR_TRWR_Pos) |
						(OSPI_HYPERRAM_LATENCY << OCTOSPI_HLCR_TACC_Pos) |
						OCTOSPI_HLCR_LM;
 
	/* CR: clear FMODE -> exit MM for now */
	OCTOSPI2->CR 	&= ~OCTOSPI_CR_FMODE;
 
	/* DCR1: Hyperbus from register access to memory */
	OCTOSPI2->DCR1 	&= ~OCTOSPI_DCR1_MTYP_0;
 
	/* CCR & WCCR:
	 *	DQS signal enabled (used as RWDS)
	 *	DTR mode enabled on address and data
	 *	address and data on 8 lines
	 */
	/* READ: CCR */
	OCTOSPI2->CCR 	= 	OCTOSPI_CCR_DQSE |
						OCTOSPI_CCR_DDTR | OCTOSPI_CCR_DMODE_2 |
						OCTOSPI_CCR_ADSIZE | OCTOSPI_CCR_ADDTR | OCTOSPI_CCR_ADMODE_2;
 
	/* WRITE: WCCR */
	OCTOSPI2->WCCR 	= 	OCTOSPI_CCR_DQSE |
						OCTOSPI_WCCR_DDTR | OCTOSPI_WCCR_DMODE_2 |
						OCTOSPI_WCCR_ADSIZE | OCTOSPI_WCCR_ADDTR | OCTOSPI_WCCR_ADMODE_2;
 
	/* DLR: data length = 1 byte */
	OCTOSPI2->DLR 	= 0;
 
	/* AR: address reset */
	OCTOSPI2->AR 	= 0;
 
	/* update state */
	hOspi2.State = HAL_OSPI_STATE_CMD_CFG;
 
	/* LPTR: lo-power timeout reset */
	OCTOSPI2->LPTR 	= 0;
 
/* HW IO MUX setup */
	/* MUX OCTOSPIM->PCR[n] */
	OCTOSPI2->CR 	&= ~OCTOSPI_CR_EN;
	/* NO multiplexed mode */
	OCTOSPIM->CR 	= 0;
	/* PORT 2:
	 *	select signals & enable
	 *	hi port 2 4..7
	 *	lo port 2 0..3
	 *	NCS 2
	 *	DQS 2
	 *	clock 2
	 */
	OCTOSPIM->PCR[1] = ( 	OCTOSPIM_PCR_IOHSRC_1 | OCTOSPIM_PCR_IOHSRC_0 | OCTOSPIM_PCR_IOHEN |
							OCTOSPIM_PCR_IOLSRC_1 | OCTOSPIM_PCR_IOLEN |
							OCTOSPIM_PCR_NCSSRC | OCTOSPIM_PCR_NCSEN |
							OCTOSPIM_PCR_DQSSRC | OCTOSPIM_PCR_DQSEN |
							OCTOSPIM_PCR_CLKSRC | OCTOSPIM_PCR_CLKEN );
 
/* DELAY block */
	/* disable the output clock and enable the access to the phase selection SEL[3:0] */
	DLYB_OCTOSPI2->CR 	= DLYB_CR_SEN;
	/* set delay */
	DLYB_OCTOSPI2->CFGR = 0 & DLYB_CFGR_SEL_Msk;
	/* disable the access to the phase selection, enable output */
	DLYB_OCTOSPI2->CR 	= DLYB_CR_DEN;
 
	/* enable in peripheral -> clear bypass */
	OCTOSPI2->DCR1 &= ~OCTOSPI_DCR1_DLYBYP;
 
/* clear all status flags */
	OCTOSPI2->FCR = 0xFFFFFFFF;
 
/* CR: memory-mapped, no timeout */
	OCTOSPI2->CR 	&= ~OCTOSPI_CR_TCEN;
	OCTOSPI2->CR 	|= OCTOSPI_CR_FMODE;
/* CR: enable peripheral */
	OCTOSPI2->CR |= OCTOSPI_CR_EN;
 
	/* set state (for DMA & HAL stuff) */
	hOspi2.State = HAL_OSPI_STATE_BUSY_MEM_MAPPED;
 
	return u8RetVal;
}
 
 
/* basic GPIO & DMA init */
void HAL_OSPI_MspInit(OSPI_HandleTypeDef *phOspi)
{
	GPIO_InitTypeDef GPIO_InitStruct = { 0 };
 
	if( phOspi->Instance == OCTOSPI2 )
	{
		/* OCTOSPI2 clock enable */
		__HAL_RCC_OCTOSPIM_CLK_ENABLE();
		__HAL_RCC_OSPI2_CLK_ENABLE();
 
		/* reset */
		__HAL_RCC_OSPI2_FORCE_RESET();
		__HAL_RCC_OSPI2_RELEASE_RESET();
 
		__HAL_RCC_GPIOG_CLK_ENABLE();
		__HAL_RCC_GPIOF_CLK_ENABLE();
		/**OCTOSPI2 GPIO Configuration
			PF0 	------> OCTOSPIM_P2_IO0
			PF1 	------> OCTOSPIM_P2_IO1
			PF2 	------> OCTOSPIM_P2_IO2
			PF3 	------> OCTOSPIM_P2_IO3
			PF4 	------> OCTOSPIM_P2_CLK
			PF12	------> OCTOSPIM_P2_DQS
			PG0 	------> OCTOSPIM_P2_IO4
			PG1 	------> OCTOSPIM_P2_IO5
			PG10	------> OCTOSPIM_P2_IO6
			PG11	------> OCTOSPIM_P2_IO7
			PG12	------> OCTOSPIM_P2_NCS
		*/
 
		GPIO_InitStruct.Mode 		= GPIO_MODE_AF_PP;
		GPIO_InitStruct.Pull 		= GPIO_NOPULL;
		GPIO_InitStruct.Speed 		= GPIO_SPEED_FREQ_VERY_HIGH;
 
		GPIO_InitStruct.Pin 		= 	OCSPI2_IO1_Pin | OCSPI2_IO0_Pin |
										OCSPI2_IO2_Pin | OCSPI2_CLK_Pin |
										OCSPI2_IO3_Pin | OCSPI2_DQS_Pin;
		GPIO_InitStruct.Alternate 	= GPIO_AF9_OCTOSPIM_P2;
		HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
 
		GPIO_InitStruct.Pin 		= OCSPI2_IO7_Pin | OCSPI2_IO5_Pin | OCSPI2_IO4_Pin;
		GPIO_InitStruct.Alternate 	= GPIO_AF9_OCTOSPIM_P2;
		HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
 
		GPIO_InitStruct.Pin 		= OCSPI2_IO6_Pin | OCSPI2_NCS_Pin;
		GPIO_InitStruct.Alternate 	= GPIO_AF3_OCTOSPIM_P2;
		HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
	}
}

ChahinezC
Lead

Hello @AAree.1​,

Unfortunately I can not specify the root cause of the issue, but I will try to provide general recommendations that might help :

  • Please ensure that all the instructions of data cache are disabled and check if the problem persists.
  • Please make sure you are respecting the timings of the memory's datasheet.
  • Please check the configuration of the OCTOSPIM if used.
  • Try working with low frequencies and check if the problem persists.
  • When generating the code with STM32CubeMX please check the alternate functions generated.

Thank you.

Best regards,

Chahinez.

rk_iot
Associate III

Hi LCE,

we are trying to using your sample code but the values of the interesting defines OSPI_HYPERRAM_RW_REC_TIME, OSPI_HYPERRAM_LATENCY, etc are missing.

Could you also post the values of these defines so we could test the sample code?

 

Thanks in advance

best regards

RK_IOT