2015-07-01 08:36 AM
Hello,
I used to be happy with fatfs and cubemx (probably a little more with fatfs rather than cubemx).In 4.8, cubemx include a file called ''fatfs.c'' that cannot be compiled because inexistant. ''fatfs'' may be a directory name but has never been a *.c file name.2015-07-01 08:44 AM
I was in the wrong, v4.8 does generates a fatfs.c file. But I had to select ''copy all used libs into project folder''. ''Copy only the necessary files'' does not copy ALL the necessary files.
2015-07-17 07:24 AM
Hello,
We do not reproduce your issue. The file you are looking for is under : Middlewares\Third_Party\FatFs\src\drivers. Depending on your choice of project settings to copy or to reference the library files, the files are either copied in your project directory or only kept as references, left in your cube repository (see in C:/users/<your username>/STM32Cube/Repository). Best regards