2016-11-07 3:19 AM
When regenerating code (previously correctly generated several times) CubeMX displays an error window and deletes an initialization assembler source file which prevents the Eclipse/System Workbench project to build successfully.
The text on the window says ''The Code is successfully generated under C:/..... but SW3STM32Project generation have a problem.'' The deleted assembly file is Drivers/CMSIS/Device/ST/STM32F0xx/Source/Templates/gcc/startup_stm32f051x8.s I have attached the .ioc file for reference #!cubemx-!code-generation2016-11-11 4:57 AM
Dear User,
Please note that your issue is reported internally for checking and we will contact you soon. Best Regards STM32.forum2016-11-23 2:08 AM
It happened again. I was using a new project which did not show the problem. Just after I checked the box ''Delete previously generated files when not re-generated'' CubeMX shows the same error window and deletes the assebnly initialization file. This is really annoying.
Unchecking the box does not change the behavior of CubeMX: this .ioc can not be used in the same place anymore.2016-11-23 8:22 AM
I am attaching the .ioc file of today's error and the log of the error obtaining making cubemx run in interactive mode
________________ Attachments : cubemx_console.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzM6&d=%2Fa%2F0X0000000bNA%2F.haI_ccdGH8w9c0q5k1G7vqoo2chACDHBCAuiOlF0Pw&asPdf=falsedecode_tag.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzWm&d=%2Fa%2F0X0000000bNB%2FSwFR45JQjzscMI1IMTXAnKuX9VJI_LGWOZYjJ9s6i8Q&asPdf=false2017-01-27 8:09 AM
Hello
Melis.Adriano
,A similar bug has been fixed in 4. Since, the 4.19 has been released.
Could you please try with that newest version ?
Great thanks in advance.
Kind regards
Marc
2017-11-30 2:45 PM
I can confirm this for version 4.19 too.
This appears to be due to a missing .xml file that accompanies the .ioc file (it has the same name as the .ioc file).
I found this out after renaming the .ioc file.
Solution:
a) Rename the .xml file as well
or
b) Undelete/recover the .xml file
or
c) Copy another such .xml file and edit it to fit the .ioc project (it contains project, MCU and debug interface name)