2016-06-24 04:59 PM
My UART interface was working great under CubeMx 4.14 with STM32F7 library v1.3. There are a lot of changes to the UART HAL (not mentioned in the release notes for CubeMx, and there are no release notes for CubeF7) in the v1.4 release. ST even changed a structure member name from State to gState. I thought this might be the only issue, but my UART interface does not work at all under the new configuration. I am really growing weary of 'upgrades' causing things to break. Looking at the Hal code, there are significant changes between the two versions. Sure would be nice to know what they were trying to 'fix'. The CubeMx interface is suppoed to save developers time, not cause them to waste days trying to figure out why a working application no longer works simply from updating CubeMX.
2016-06-25 08:28 AM
What makes me sad is that if half the effort put behind HAL had been applied to building a middleware library around SPL we'd be miles ahead...
2016-06-29 03:04 PM
I'm seeing this same effect after updating to firmware 1.12.0 on STM32F4.
The transmit section seems to be working properly, but receive generates noise errors (NF) and framing errors (FE).(whining about the SPL going away will not bring it back, move on)2016-07-03 02:57 AM
Same here, with STM32F4 and new FW 1.12.0
I'm using DMA mode for Rx and Tx. Code seens to run, but nothing is sent through UART. Nothing is receive too. I checked signal with logic analyzer.2016-07-03 06:41 AM
Well you enjoy your support/regression nightmare, I've moved down a different path already.
2016-07-04 12:30 AM
''I've moved down a different path already.''
Is that anything the rest of us could benefit from? I've been persevering with the most current SPL for STM32F4 V1.7.0.2016-07-04 01:29 AM
> I've been persevering with the most current SPL for STM32F4 V1.7.0.
Unfortunately, this is no such option for ''later'' MCUs, including the F7 line, where no SPL exists. From earlier posts, I conclude clive speaks about direct-register-access. I'm doing the same for F7, using parts of the awkward Cube SW as template. The hyped LL part seem but a sorry stub there - except I'm overlooking something. I can see it more relaxed, using STM32 only for hobby projects. My company had chosen a different Cortex M vendor years ago.