2024-03-24 7:58 AM
Hi :
I updated STM32CubeIDE a few hours ago.
Version: 1.15.0
Build: 20695_20240315_1429 (UTC)
Now it will failed at the SystemClock_Config() and missing arm_sorting.h
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE3) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 16;
RCC_OscInitStruct.PLL.PLLP = 8;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) ----> failed here
{
Error_Handler();
}
/** Initializes the CPU, AHB, and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
here are the details
Dev Board Nucleo-U5A5ZJ-Q
Name : Error_Handler
Details:{void (void)} 0x800068c <Error_Handler>
Default:{void (void)} 0x800068c <Error_Handler>
Decimal:-128
Hex:0x80
Binary:10000000
Octal:0200
I have no such error before update.
Any idea how to resolve this?
Simon
2024-03-26 3:53 AM
You have mentioned earlier regarding something about the path:
here is the link:
https://github.com/ARM-software/CMSIS_5/issues/910
below is the comment:
"You need to include the folder DSP/PrivateInclude when building.
This folder contains headers that are used only for building the libraries but not to use it.
The other folder DSP/Include is for headers which are needed to use the library. "
I can locate the arm_sorrting.h header files as mentioned in the link.
You did mentioned about path, build path ? if yes where can I check and probably change it?
Best Regards
Simon
2024-03-28 4:02 AM
hi @STTwo-32 :
I get passed the " SystemClock_Config()" but now it stop at MX_USB_OTG_HS_HCD_Init().
static void MX_USB_OTG_HS_HCD_Init(void)
{
/* USER CODE BEGIN USB_OTG_HS_Init 0 */
/* USER CODE END USB_OTG_HS_Init 0 */
/* USER CODE BEGIN USB_OTG_HS_Init 1 */
/* USER CODE END USB_OTG_HS_Init 1 */
hhcd_USB_OTG_HS.Instance = USB_OTG_HS;
hhcd_USB_OTG_HS.Init.Host_channels = 16;
hhcd_USB_OTG_HS.Init.speed = HCD_SPEED_HIGH;
hhcd_USB_OTG_HS.Init.dma_enable = DISABLE;
hhcd_USB_OTG_HS.Init.phy_itface = USB_OTG_HS_EMBEDDED_PHY;
hhcd_USB_OTG_HS.Init.Sof_enable = DISABLE;
hhcd_USB_OTG_HS.Init.low_power_enable = DISABLE;
hhcd_USB_OTG_HS.Init.use_external_vbus = ENABLE;
if (HAL_HCD_Init(&hhcd_USB_OTG_HS) != HAL_OK) ----> it hang up here.
{
Error_Handler();
}
/* USER CODE BEGIN USB_OTG_HS_Init 2 */
/* USER CODE END USB_OTG_HS_Init 2 */
}
it hang at
if (HAL_HCD_Init(&hhcd_USB_OTG_HS) != HAL_OK)
{
Error_Handler();
}
Do you think it is about setting?
Best Regards
Simon