cancel
Showing results for 
Search instead for 
Did you mean: 

Cube IDE Version: 1.15.0 failed at SystemClock_Config()

S_Ong
Associate III

Hi :

      I updated  STM32CubeIDE a few hours ago.

Version: 1.15.0

Build: 20695_20240315_1429 (UTC)

 

Now it will failed at the SystemClock_Config() and missing arm_sorting.h

 

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 

/** Configure the main internal regulator output voltage

*/

if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE3) != HAL_OK)

{

Error_Handler();

}

 

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;

RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;

RCC_OscInitStruct.PLL.PLLM = 1;

RCC_OscInitStruct.PLL.PLLN = 16;

RCC_OscInitStruct.PLL.PLLP = 8;

RCC_OscInitStruct.PLL.PLLQ = 2;

RCC_OscInitStruct.PLL.PLLR = 2;

RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;

RCC_OscInitStruct.PLL.PLLFRACN = 0;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) ----> failed here

{

Error_Handler();

}

 

/** Initializes the CPU, AHB, and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2

|RCC_CLOCKTYPE_PCLK3;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

{

Error_Handler();

}

}

 here are the details

 Dev Board Nucleo-U5A5ZJ-Q

 

Name : Error_Handler

Details:{void (void)} 0x800068c <Error_Handler>

Default:{void (void)} 0x800068c <Error_Handler>

Decimal:-128

Hex:0x80

Binary:10000000

Octal:0200

 

S_Ong_0-1711292059277.png

I have no such error before update.

Any idea how to resolve this?

 

Simon

11 REPLIES 11
STTwo-32
ST Employee

Hello @S_Ong 

Could you share your project here. I think you should update your paths. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

S_Ong
Associate III

Hi @STTwo-32 :

                          Sure, do you need the whole file in zip? FYI I, installed the Cube IDE Version: 1.15.0 in another new laptop, and it has the same problem. But with the same laptop installed with the earlier version, the project ran without error.  Please let me know how to share the project.

 

Best Regards.

 

Simon

 

 

 

 

Hello, you have just to share the project in any one of the supported formats.

Best regards.

STTwo32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

S_Ong
Associate III

Hi @STTwo-32 :

S_Ong_2-1711373737811.png

 

 

S_Ong_0-1711373686256.png

S_Ong_3-1711373774344.png

S_Ong_4-1711373956876.png

 

I don't see any  "arm_sorting.h" at both folders. 

"dsp/support_functions.h" yes, the support_functions header file is in both folder.

is this what you are looking for?

 

Regards and Thanks

 

Simon

 

 

 

S_Ong
Associate III

Hello @STTwo-32 :

Please bear with me, I am new to this community. Here is the main.c

 

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include <stdio.h> /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ PCD_HandleTypeDef hpcd_USB_OTG_HS; /* USER CODE BEGIN PV */ uint16_t counter=0; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void SystemPower_Config(void); static void MX_GPIO_Init(void); static void MX_ICACHE_Init(void); static void MX_USB_OTG_HS_PCD_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ int _write(int file, char *ptr, int len) { (void)file; int DataIdx; for (DataIdx = 0; DataIdx < len; DataIdx++) { // __io_putchar(*ptr++); ITM_SendChar(*ptr++); } return len; } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* Configure the System Power */ SystemPower_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_ICACHE_Init(); MX_USB_OTG_HS_PCD_Init(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ printf("Counter Value "); HAL_Delay(10000); } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE3) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1; RCC_OscInitStruct.PLL.PLLM = 1; RCC_OscInitStruct.PLL.PLLN = 16; RCC_OscInitStruct.PLL.PLLP = 8; RCC_OscInitStruct.PLL.PLLQ = 2; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1; RCC_OscInitStruct.PLL.PLLFRACN = 0; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_PCLK3; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief Power Configuration * @retval None */ static void SystemPower_Config(void) { HAL_PWREx_EnableVddIO2(); /* * Disable the internal Pull-Up in Dead Battery pins of UCPD peripheral */ HAL_PWREx_DisableUCPDDeadBattery(); /* * Switch to SMPS regulator instead of LDO */ if (HAL_PWREx_ConfigSupply(PWR_SMPS_SUPPLY) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN PWR */ /* USER CODE END PWR */ } /** * @brief ICACHE Initialization Function * @param None * @retval None */ static void MX_ICACHE_Init(void) { /* USER CODE BEGIN ICACHE_Init 0 */ /* USER CODE END ICACHE_Init 0 */ /* USER CODE BEGIN ICACHE_Init 1 */ /* USER CODE END ICACHE_Init 1 */ /** Enable instruction cache in 1-way (direct mapped cache) */ if (HAL_ICACHE_ConfigAssociativityMode(ICACHE_1WAY) != HAL_OK) { Error_Handler(); } if (HAL_ICACHE_Enable() != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ICACHE_Init 2 */ /* USER CODE END ICACHE_Init 2 */ } /** * @brief USB_OTG_HS Initialization Function * @param None * @retval None */ static void MX_USB_OTG_HS_PCD_Init(void) { /* USER CODE BEGIN USB_OTG_HS_Init 0 */ /* USER CODE END USB_OTG_HS_Init 0 */ /* USER CODE BEGIN USB_OTG_HS_Init 1 */ /* USER CODE END USB_OTG_HS_Init 1 */ hpcd_USB_OTG_HS.Instance = USB_OTG_HS; hpcd_USB_OTG_HS.Init.dev_endpoints = 9; hpcd_USB_OTG_HS.Init.speed = PCD_SPEED_HIGH; hpcd_USB_OTG_HS.Init.phy_itface = USB_OTG_HS_EMBEDDED_PHY; hpcd_USB_OTG_HS.Init.Sof_enable = DISABLE; hpcd_USB_OTG_HS.Init.low_power_enable = DISABLE; hpcd_USB_OTG_HS.Init.lpm_enable = DISABLE; hpcd_USB_OTG_HS.Init.use_dedicated_ep1 = DISABLE; hpcd_USB_OTG_HS.Init.vbus_sensing_enable = DISABLE; hpcd_USB_OTG_HS.Init.dma_enable = DISABLE; if (HAL_PCD_Init(&hpcd_USB_OTG_HS) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USB_OTG_HS_Init 2 */ /* USER CODE END USB_OTG_HS_Init 2 */ } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LED_RED_GPIO_Port, LED_RED_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LED_GREEN_GPIO_Port, LED_GREEN_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, UCPD_DBn_Pin|LED_BLUE_Pin, GPIO_PIN_RESET); /*Configure GPIO pin : PC13 */ GPIO_InitStruct.Pin = GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /*Configure GPIO pin : VBUS_SENSE_Pin */ GPIO_InitStruct.Pin = VBUS_SENSE_Pin; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(VBUS_SENSE_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : UCPD_FLT_Pin */ GPIO_InitStruct.Pin = UCPD_FLT_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(UCPD_FLT_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : PB15 */ GPIO_InitStruct.Pin = GPIO_PIN_15; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /*Configure GPIO pin : LED_RED_Pin */ GPIO_InitStruct.Pin = LED_RED_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LED_RED_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : LED_GREEN_Pin */ GPIO_InitStruct.Pin = LED_GREEN_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LED_GREEN_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : T_VCP_TX_Pin T_VCP_RX_Pin */ GPIO_InitStruct.Pin = T_VCP_TX_Pin|T_VCP_RX_Pin; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF7_USART1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : PA15 */ GPIO_InitStruct.Pin = GPIO_PIN_15; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pins : UCPD_DBn_Pin LED_BLUE_Pin */ GPIO_InitStruct.Pin = UCPD_DBn_Pin|LED_BLUE_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more

 

Regards

 

Simon

Could you please Compress your project and add it as attachment to this post.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

S_Ong
Associate III

@STTwo-32 :

                   How to attach files? I don't see any selection for files attachment .

Best Regards

simon

S_Ong
Associate III

@STTwo-32 :

                       My apologies :grinning_face_with_sweat:. Here is the attached files

I've personally test it and it works perfectly for me. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.