2021-11-18 3:23 AM
Hy,
I would like to create a simple Custom cards using STM32L562.
My first question is:
Do you have a simple schematic with only essentials components ?
And my second is:
at the first initialisation, the MCU need a BOOTLOAD or particular manipulation (hardware and software) ?
I have tried to create my custom cards but i have the problem to initialized this.
Thank's in advance.
2021-11-18 4:50 AM
The NUCLEO board schematics should be relatively simple and mundane. Pull those via the CAD Resources tab of the product page.
Pull BOOT0 pin low to ensure the internal loader runs code in FLASH in normal operation.
Connect VDDA/VDDA as the power reset circuitry and PLL
Export the debug pins along with NRST, and a USART for diagnostics and programming, see App Note An2606
2021-11-18 5:20 AM
Here is a reference for hardware layout:
> I have tried to create my custom cards but i have the problem to initialized this.
What problem are you running into?
2021-11-18 5:47 AM
thank's for your answers,
I think my real problem is at the first initialisation "bootload manipulation", I load my program to the different STM32L562 sometime it's works at the first time and sometime no, but after debuging with test point sometime it's work (like magic but not magic :>) .
I suppose differents problems :