2021-11-28 1:08 PM
Hello everyone.
I have 2 incremental encoders. One of them has the output voltage of signals A and B 5 volts and the other one 24 volts.
I need to count the increments with stm32f4 and timers in the mode encoder.
But I have to first convert the 5 and 24 volts to 3.3.
Can I use a comparator like LM393? Does it support high frequency of the encoder?
Or do you have any other suggestions? I also tried Voltage Divider but it didn't work.
Thank you so much.
Solved! Go to Solution.
2021-11-29 1:01 AM
You can convert either with a level shifter, or with a comparator you mentioned (of course with suitable dimensioning). It depends on the frequency of the encoder signal what is to be used, e.g. type of comparator.
A simple voltage divider will not work for various reasons, including because capacitive effects distorting the signal, and the encoder has an output resistance that must be taken into account.
Regards
/Peter
2021-11-29 1:01 AM
You can convert either with a level shifter, or with a comparator you mentioned (of course with suitable dimensioning). It depends on the frequency of the encoder signal what is to be used, e.g. type of comparator.
A simple voltage divider will not work for various reasons, including because capacitive effects distorting the signal, and the encoder has an output resistance that must be taken into account.
Regards
/Peter