2015-10-27 4:28 AM
I am Facing a problem to use TMR2 and SPI3 in STM32F103. I am using Keil Software to write the code and the Problem is if i remap and choose SPI1 TMR2 will stop working and if i stop using the remapped SPI1; the remapped TMR2 will work. The pins i am using for the Remapped SPI1 is PB3/B4/B5 and the pin that i am using for the remapped TMR2 is PA15. This is a sample code for how i am declaring these pins:
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA |RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC | RCC_APB2Periph_SPI1 | RCC_APB2Periph_AFIO, ENABLE );
GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
GPIO_PinRemapConfig(GPIO_PartialRemap1_TIM2,ENABLE);
GPIO_PinRemapConfig (GPIO_Remap_SPI1, ENABLE);
#spi1 #stm32f103r8 #tmr22015-10-27 5:45 AM
May be you should consider a different STM32 family that permits PIN level peripheral configuration? The F1 uses a course block level for groups of pins, and this can be significantly more difficult to escape all the peripherals in the manner you want.