2023-05-19 10:57 AM
2023-05-19 1:39 PM
Depends on your package, but your options are limited, search the data sheet.
For Dual Bank QSPI in parallel you don't need two CS, other STM32 have an alternate pin for this too (thinking H7Ax)
Could you use SDMMC2 instead ?
2023-05-20 1:06 AM
Thank you for your help if i have no choice i going to try sdmmc2 but i very hard to build a clear pin out in cube mx in order to make a pcb full functional
2023-05-20 6:23 AM
How are you configuring QSPI that needs two chip selects?
The most practical use cases require a pair of identical devices on the bus to double the bandwidth. I don't think it can handle two different devices if one is in memory-mapped mode.