2014-07-01 6:20 PM
Hi,
I want to haveSTM32F4 Discovery as SPI slave and PIC18F2580 as SPI master. I tried to modify examples found on the internet to suit my need, but none of them work. I haveneither access to oscilloscope nor logic analyzer, so it's very difficult for me to understand why the code doesn't work. The following is configuration I'm using for PIC (Master mode): Note: I used this configuration for mastertomake communicationbetween 2 PICs and it worked./* SMP: Sample bit
* SPI Master mode:
* 1 = Input data sampled at end of data output time
* 0 = Input data sampled at middle of data output time
* SPI Slave mode:
* SMP must be cleared in slave mode
*/
#define _SMP 0
/* CKE: SPI Clock Select bit
* 1 = Transmit occurs on transition from active to idle clock state
* 0 = Transmit occurs on transition from idle to active clock state
*/
#define _CKE 0
/* CKP: Clock Polarity Select bit
* 1 = Idle state for clock is a high level
* 0 = Idle state for clock is a low level
*/
#define _CKP 1
/* Synchronous Serial Port Mode Select bits
* 0101 = Slave mode, clock = SCK pin, SS pin disabled (can be used as I/O pin)
* 0100 = Slave mode, clock = SCK pin, SS pin enabled
* 0011 = Master mode, clock = TMR2 output/2
* 0010 = Master mode, clock = Fosc/64
* 0001 = Master mode, clock = Fosc/16
* 0000 = Master mode, clock = Fosc/4
*/
#define _SSPM_MASTER 0b0000
void
SPI_init() {
TRISA = 0x00;
/* set all port A pins as output pins */
ADCON1 = 0x0F;
/* set all port A pins, including SS (RA5), as digital I/O */
TRISC = 0b00010000;
/* Set SCK pin (RC3) as output
* SDI pin (RC4) as input
* SDO pin (RC5) as output */
SSPSTAT = 0b00000000;
/* Initialize SSPSTAT register to POR state */
SSPSTATbits.SMP = _SMP;
/* Configure sample bit */
SSPSTATbits.CKE = _CKE;
/* Configure clock select bit */
SSPCON1 = 0b00000000;
/* Initialize SSPCON1 register to POR state */
SSPCON1bits.CKP = _CKP;
/* Configure clock polarity select bit */
SSPCON1bits.SSPEN = 1;
/* Enable SPI (set SCK, SDO, SDI, and SS as serial port pins)*/
SSPCON1bits.SSPM = _SSPM_MASTER;
/* Configure sync mode bits for master */
}
And this is theconfiguration I'm using for STM32F4 Discovery (Slave mode):
void
init_SPI1(
void
) {
GPIO_InitTypeDef GPIO_InitStruct;
SPI_InitTypeDef SPI_InitStruct;
// enable clock for used IO pins
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
/* configure pins used by SPI1
* PA5 = SCK
* PA6 = MISO
* PA7 = MOSI
*/
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_6 | GPIO_Pin_5;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStruct);
// connect SPI1 pins to SPI alternate function
GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1);
// enable clock for used IO pins
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE);
// enable peripheral clock
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);
/*
* CPOL = 1 --> clock is high when idle
* CPHA = 0 --> data is sampled at the first edge
*/
SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
// set to full duplex mode, seperate MOSI and MISO lines
SPI_InitStruct.SPI_Mode = SPI_Mode_Slave;
// transmit in slave mode
SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b;
// one packet of data is 8 bits wide
SPI_InitStruct.SPI_CPOL = SPI_CPOL_High;
// clock is high when idle
SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge;
// data sampled at first edge
SPI_InitStruct.SPI_NSS = SPI_NSS_Soft;
// set the NSS management to internal and pull internal NSS high
SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_LSB;
// data is transmitted MSB first
SPI_Init(SPI1, &SPI_InitStruct);
SPI_Cmd(SPI1, ENABLE);
// enable SPI1
}
I'm connecting
- SCK (PA5) to PIC's SCK (RC3)
- MISO (PA6) to PIC's SDI (RC4)
- MOSI (PA7) to PIC's SDO (RC5)
Any help would be highly appreciated. Thank you in advance for your suggestions and sorry for my bad English.
Best Regards,
Pat