cancel
Showing results for 
Search instead for 
Did you mean: 

Compiling error.

phuocnguyenhuu96
Associate III

Hi.

Have you ever compile code with error: More than one section matches selector - cannot all be FIRST/LAST.

I searching on google I see that the error because when appear two file same startup_stm32f746xx.s in Startup file and Divice File. I'm delete one file in Start up file and compile again but it's doesn't work.

Please help me with this problem.

Thank you so much.

3 REPLIES 3

This is going to be hard to diagnose without looking at the project, the files inside, and the scatter file

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
phuocnguyenhuu96
Associate III

Thank you for your support. I complete to solve this problem.

henry.dick
Senior II

"I complete to solve this problem."

nice. that's going to be very helpful to the next person running into this problem.