2018-07-27 11:48 AM
Hi.
I'm reading Incremental Optic encoder with Timer3. The counter value is 4095 when the encoder rotates one turn. My goal is to produce pulses from 0-25ms through another timer when the Encoder turns half a turn.
In order to do this, I am trying to trigger Timer2 via Timer3. But I couldn't run
This is Encoder Timer Settings
void Encoder_Init(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE);
// Step 1: Initialize GPIO as input for rotary encoder
//PA6 (TIM3_CH1) (encoder pin A), PA7 (TIM3_CH2) (encoder pin B)
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up | TIM_CounterMode_Down;
TIM_TimeBaseStructure.TIM_Period = 4095;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
/* Output Compare Active Mode configuration: Channel1 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = 1000;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM3, &TIM_OCInitStructure);
TIM_SetCounter(TIM3,0);
TIM_EncoderInterfaceConfig(TIM3, TIM_EncoderMode_TI12, TIM_ICPolarity_Rising, TIM_ICPolarity_Rising);
TIM_SelectOutputTrigger(TIM3,TIM_TRGOSource_OC1Ref);
TIM_Cmd(TIM3, ENABLE);
}Slave Timer settings
void SlaveTimerInit(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
GPIO_InitTypeDef GPIO_InitStruct;
// Enable clock
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0;
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_Init(GPIOA, &GPIO_InitStruct);
// Time Base configuration
TIM_TimeBaseStructure.TIM_Prescaler = 72-1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStructure.TIM_Period = 0xFFFF;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
/* TIM2 PWM2 Mode configuration: Channel1 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = 20000; //20ms
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM2, &TIM_OCInitStructure);
/* One Pulse Mode selection */
TIM_SelectOnePulseMode(TIM2, TIM_OPMode_Single);
/* Input Trigger selection */
TIM_SelectInputTrigger(TIM2, TIM_TS_ITR0);
/* Slave Mode selection: Trigger Mode */
TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Trigger);
}Where am I making mistakes? Thanks. How to do it?
2018-07-27 1:06 PM
What part specifically are you using?
What routing does the Reference Manual for your part indicate is available?
2018-07-27 10:51 PM
I looked at the Reference Manual, but I could not figure out what direction to do. First, is this Possible? Could you give me an example?
2018-07-28 7:38 AM
you either implement that in spl/hal, or just change the smcr register.