cancel
Showing results for 
Search instead for 
Did you mean: 

Compatibility of STM32H5 with STEVAL-MKI227KA Kit

Azad
Associate II

Is it possible to use any STM32 microcontroller, particularly the STM32H5, with the STEVAL-MKI227KA evaluation kit that based on LSM6DSV16X sensor? I’ve only found information regarding the STM32F4.

1 ACCEPTED SOLUTION

Accepted Solutions
Andrew Neil
Evangelist III

Of course it is.

The LSM6DSV16X sensor neither knows nor cares what microcontroller you use - all it sees is the SPI / I²C / MIPI I3C interface.

View solution in original post

3 REPLIES 3
Andrew Neil
Evangelist III

Of course it is.

The LSM6DSV16X sensor neither knows nor cares what microcontroller you use - all it sees is the SPI / I²C / MIPI I3C interface.

Azad
Associate II

Thanks for clarifying this issue. I have one more question, is the STEVAL-MKI227KA physically compatible with the NUCLEO-H503RB in terms of pin connections? 

You'd have to look at the schematics for that.

But the STEVAL-MKI227KA is a standard DIL 24 package:

AndrewNeil_0-1722937170270.png

https://www.st.com/en/evaluation-tools/steval-mki227ka.html

 

The NUCLEO-H503RB doesn't have a DIP-24 socket on it:

 

AndrewNeil_2-1722937275310.png

https://www.st.com/en/evaluation-tools/nucleo-h503rb.html

So you're going to have to use flying leads, or make/buy an adaptor; eg,

AndrewNeil_3-1722937466325.png