cancel
Showing results for 
Search instead for 
Did you mean: 

Compatibility of different footprints of same MCU type

Exit0815
Senior

Hello,

I want to change the MCU STM32F779AIY to STM32F779NIH6

I already checked the pinout in CubeMX and i can use the same config for the peripherals at the same naming of pins (PB1, PA4 and so on).

Do i need to change anything at the software if i change the MCU?

As i can see so far, the software does not detect the type of the MCU, as long as GPIO stuff is the same (which is) it will work. Am i right here?

 

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Correct, for this swap you won't have to change the code at all. They are effectively the same exact chip in a different package.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

Correct, for this swap you won't have to change the code at all. They are effectively the same exact chip in a different package.

If you feel a post has answered your question, please click "Accept as Solution".