2020-07-20 7:30 AM
Hello,
I am trying to communicate with interrupt between the Cortex M4 and M7. I tested the HSEM but, maybe I'm wrong, the semaphore locks a process when it waits for it.
Thanks for you help
2020-07-20 7:43 AM
One core can do a fast take and immediate release of an unlocked semaphore which can cause a release interrupt in the other core. No blocking, just set a flag in the isr. Also, one core can start a mdma transfer to/from f7 tcram to d2 ram and the finished mdma transfer can interrupt the other core, so there is also a nonblocking way to copy data from one to the other.
2020-07-20 7:50 AM
Okkk i will try, thank you very much for your fast reply !!!
2020-07-24 4:53 AM
Have you some examples of hsem with interrupt please ?