2015-04-28 04:52 AM
Hello,there!
I want to generate code base on model by simulink and stm32cubeMX.I install the ''target support package-stm32 adapter'' in simulink and stm32cubeMX version 4.70 in computer.I set a model in simulink and drag a MCU config block in it,then I select the .ioc file which was generated in stm32cubeMX.I chose the stm32f0803 discovery board,and configue the ADC peripheral in stm32cubeMX.2015-10-06 10:04 AM
Hi mingming.xu,
Upgrade STM32-MAT/TARGET and STM32CubeMx with latest versions. -Shahrzad-