cancel
Showing results for 
Search instead for 
Did you mean: 

Code for STM32F779I Eval board

yalamanda dosakayala
Associate II
Posted on January 06, 2018 at 08:53

Hi STM Community, I am currently working on STM32F779I eval board for developing CAN, FreeRTOS with FatFs and SD card drivers.I have generated code using cube mx and imported into system workbench for STM32 IDE.

I tried to test the code for writing into SD card , But it is failing at fmount .

Then I tried Example code(Fatfs_uSD_RTOS) available for F769I  eval board ,I build and flashed to F779I board, It is able to write to SD card successfully.

So I have doubt  that what is the difference between these two eval boards, if no much differences are available can i use these code for f779i board for my further development. If not what are the changes I have to make f769i code.

As mentioned in one of the post 

https://community.st.com/message/175333-building-samples-of-stm32cubef7

  . I found only encryption support is difference .

Please suggest me Whether to proceed with f769i code for f779i or else do I need to work on  the generated code for f779i cube mx.

Thanks

#stm32f7
0 REPLIES 0